News_banner

Resources

TechNexion kicks off embedded world 2020

Feb 25, 2020



For the upcoming embedded world 2020 event, TechNexion is excited to present the largest number of modules, systems and technologies ever. Among its varied embedded solutions to be exhibited, TechNexion will be highlighting a powerful lineup of new products based on NXP i.MX8M Mini, Intel Apollo Lake processors and Qualcomm QCA9377, QCA6174 chipsets.

TechNexion is highlighting two new SoM families: AXON and FLEX. AXON is a product family of small form factor (58 x 37 mm) modules designed for specialized embedded applications requiring another dimension of I/O flexibility. AXON-IMX8M-MINI is also based on NXP i.MX8M Mini applications processor and features AXON Fabric programmable logic, a specialized IC that provides additional functions including nearly infinite pinmuxing, allowing for true pin-to-pin compatibility between SoC versions. FLEX series, on the other hand, is a low-cost family making use of low-cost LPDDR4 SO-DIMM connector. FLEX-IMX8M-MINI (69.6 x 35 mm) offers HD multimedia streaming and integrated 3D graphics at a price point for cost sensitive applications. Our flagship PICO-IMX8M-MINI SoM of the widely adopted ultra-small form factor PICO family, is based on NXP i.MX8M Mini applications processor (ARM Cortex-A53 + M4 architecture), a low-power quad core processor running up to 1.8GHz with built-in 3D GPU, supporting real-time video encoding and decoding. The SoM integrates a fully certified wireless module PIXI-9377 based on Qualcomm QCA9377. PICO-IMX8M-MINI supports Android, Linux, Yocto and Ubuntu OS. This small footprint embedded module (37 x 40 mm) is a great fit for low power yet performing applications.

Furthermore, TechNexion shows off an expanded lineup of fully certified (CE / ETSI / FCC / IC / RCM / TELEC) PIXI and STIX series combo wireless communication modules based on Qualcomm QCA9377 and QCA6174 solutions. The modules are available in several M.2 and mini-PCIe form factors.

On top of that, TechNexion showcases several products based on Intel Apollo Lake processor family (Intel Atom x5-E3930, x5-E3940 or x7-E3950) that can be easily deployed in diverse industrial applications ranging from manufacturing robots and machinery, to radar and sensors on ships, trains and automobiles, to in-vehicle experience and video systems. TC series Multi Touch HMIs come in from 10.1” to 21.5” sizes. On the other hand, TCK3-APL is a ruggedized box PC fully customizable to handle your projects with IoT integration.

This year, TechNexion teams up with Xada Technologies introducing several Xada devices, that work in unison to blanket commercial or industrial space with hyper-fast, super-stable Wi-Fi, reliable and remarkably accurate sensor hubs, and control panels that can be easily installed, deployed and maintained.

Attendees can visit TechNexion’s booth in Hall 1, Booth 1-307 until Thursday, February 27. Meet our embedded experts and learn more how our latest end-to-end solutions can enable you to accelerate your IoT projects and stay ahead.

About embedded world Exhibition & Conference

At Exhibition Centre Nuremberg in February 2020, embedded systems will once again be the focus of embedded world Exhibition & Conference, the leading international fair for the sector. Embedded experts from around the world gather in Nürnberg to network and showcase their innovative solutions to meet the challenges of the future. The exhibition takes place in Nürnberg, Germany every year in February or March.

About TechNexion

TechNexion offers a wide range of embedded modular solutions to leading OEM/ODM companies in the multimedia, communication, security, automation and process control industries. TechNexion continuous investment in production technology and state-of-the-art equipment upgrades make it possible to meet technically increasingly complex customer demand. TechNexion products range from System on Modules, Connectivity Modules, Sensors, Embedded and Panel Computing Devices to IIoT Devices. All products and solutions are backed up with unmatched longevity, open hardware documentation and open source software.

TechNexion is a ISO-9001 and ISO-14001 certified company and is a founding member of the EDM (Embedded Design Modules) Standard.
For more information, visit www.technexion.com.

Get a Quote

Fill out the details below and one of our representatives will contact you shortly.

SHARE YOUR CART